When is a backup power supply required for interface protections?
Whenever the interface protection is installed as independent device from [...]
Whenever the interface protection is installed as independent device from [...]
PMVFUPS01 guarantees the necessary energy by accumulating it in capacitors, [...]
A maximum time of 15s is required to fully charge [...]
PMVFUPS01 accumulates enough energy (200Ws) to correctly drive PMVF series [...]
The Hour counter function allows to count the working hours [...]
Yes. ____________________________________________________________ Other information on this topic Visit our website [...]
No, our HMIs can communicate with all devices that have [...]
There is no predefined maximum number, theoretically it is unlimited. [...]
Yes, by default there are already three levels of access [...]
Programming in simple and fast way, ideal solution for the [...]