Considering a soft starter, how to size the line contactor?
The line contactor must be sized in AC-3 category with [...]
The line contactor must be sized in AC-3 category with [...]
Bypass contactor should be AC-1 rated for the motor full [...]
The command of the line contactor is managed automatically by [...]
Yes, it can be used circuit breaker with undervoltage trip. [...]
It is a contactor installed upstream the soft starter to [...]
Yes, it is possible to do this by making a [...]
Yes, all the parameters accessible from the display are also [...]